Hello,
I am working on a temperature sensor design based on the ADS1262 using a 2 legged Wheatstone bridge. I use my incoming supply (~+4.7V) for DVDD, AVDD and Vref (the Wheatstone source voltage). I have different decoupling caps (both 1u) on the digital and analog supply pins. Vref+ is AIN0, Vref- is AIN1, Vin+ is AIN2, Vin- is AIN3. I have placed 1u X2Y caps on the across the Vin and Vref inputs. All other inputs are unused and shorted to REFOUT. I am using the internal oscillator. I use a 4.7nF C0G cap between CAPP and CAPN. I am using SPI communication with 47R resistors inline to CS, SCLK, DIN and DOUT/DRDY. START is held to DVDD through a 47R. RESET/PWDN is connected to DVDD. I have a 1u cap to gnd from BYPASS. I have a two layer board, the entire second layer is GND.
I am communicating with 3 such circuits using the same SPI bus.
Registers are set to:
POWER: 0x10. Internal ref disabled.
INTERFACE: 0x04. Status byte enabled, checksum bit disabled.
MODE0: 0x00. Continuous conversion, chop disabled, no delay.
MODE1: 0x80. FIR filter
MODE2: 0x81. PGA bypassed, gain 1, 5 Sa/s
INPMUX: 0x23. Vin+: AIN2, VIN-: AIN3
IDACMUX: 0xBB. IDAC1, IDAC2 No Connection.
IDACMAG: 0x00. IDAC1, IDAC2 Off.
REFMUX: 0x09. VrefP: AIN0, VrefN: AIN1.
TDACP: 0x00. No connection.
TDACN:0x00. No connection.
GPIOCON:0x00. None connected.
GPIODAT:0x00. Output (default).
For my test experiment (to gather the attached data), I have replaced my temperature sensing elements with precision resistors (8k,+/- 0.01%, +/-0.2ppm/°C). My fixed leg resistors are 8.2k (+/-0.1%,+/-10ppm/°C). The goal is to establish my circuit's noise floor. I am reading data by polling with a RDATA1 command every ~0.236s (a rate roughly 4.2Hz, so I am not quite getting all 5 samples however status byte is saying that data is new). I am seeing a periodic charging and discharging with a time constant of ~1hr (4102s). The magnitude of this charging is ~20uV. It looks very much like some kind of R/L or RC periodic event but I can't identify the stimulus (must be some kind of square excitation).
Please help!!