Part Number: DAC8811
The DAC8811 datasheet specifies 50pF typical, but code dependent. Is the code dependence of the output capacitance characterized?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC8811
The DAC8811 datasheet specifies 50pF typical, but code dependent. Is the code dependence of the output capacitance characterized?
Hi Ted,
I checked with the internal team and found that we don't have any characterization data for output capacitance. Sorry for that.
Regards,
Uttam
I plan to use the the DAC8811 in a VGA with a less conventional configuration wherin the DAC is in the feedback path of the op-amp (see image below). Given that the output capacitance is code dependent, but uncharacterized, can you tell me if it is still recommended to place a capacitor from the op-amp output to the inverting input for stability (as is suggested when the DAC is followed by a TIA? If so, can you suggest a suitable capacitor value?