Other Parts Discussed in Thread: TVP5147, TVP5147M1
Hello,
I have a custom board with a TVP5147PFP. I am using this to decode a B/W PAL signal. The input PAL signal seems to drive a monitor just fine. But when the same input signal is given to the TVP5147, i get a vertical and horizontal sync signal loss from status register 0X3A and there is no output from the CLOCK, HS, FS pins. These are the settings of the TVP5147 :
a) Input given to VI_1_A (Pin 1) - Inputs are terminated with 75ohm and ac coupled through a 0.1uF capacitor.
b) All registers are at their power on defaults( i guess this means that autoswitch is enabled)
c) I2C reads from the device seems to be working fine and i am able to read CHIP ID registers successfully.
d) My clock is a fundamental 14.31818 MHz crystal with load capacitors calculated as per the datsheet recommendations.
e) Power Supplies (1.8V, 3.3V) have sufficient decoupling and am using ferrite beads for low passing the supply to remove residual ripple, if any
f) PWDN pin is pulled low and reset is proper.
g) I am using separate analog and digital grounds on my circuit board and am tying them together by means of a ferrite bead.
Could someone kindly explain if this is caused by a hardware issue or am i not configuring the TVP5147 properly ? I have verified the line and frame timings of my input signal and it seems to be fine.
Any help would be greatly appreciated. I can post scope shots of my signals and register dumps if needed...
Thanks!
Sornam