Other Parts Discussed in Thread: AFE7070
Hi,
I want to work with the AFE7070 in "Dual input clock(00)" mode. I have configured register0 value to 0xB6 or 0xB4, and there is no RF output, When I change the "data_clk_sel" to '1', it start work( their is output RF),even if I disconnect the CLK_IO signal from the input. The CLK_IO signa to the AFE7070 looks OK. Currently, I use an abnormal configuration since the value of register0 is 0xBE, anything I can do to have thi smode working?
Many Thanks,
HRi