This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: ADS130E08 Sample Code

Other Parts Discussed in Thread: ADS131E06

Hi Greg,

we have a problem with ads131e06. Some reason we can't read spi data. I think we can write ( we can start adc via spi command) . If there is any sample code we can understand what we do wrong. Can you send me ?

  • Hello Kaliptra,

    I split your thread out as an individual post so the other thread remains closed. We have code for the EVM, but it is very complicated and contains a lot of code that is totally unrelated to communicating to the ADS131E06. In addition, it is specific to the C5x DSP so I do not think it would be very useful. Instead, could you capture the SPI signals during a data read using a logic analyzer or oscilloscope and post the image here? Try to capture DRDY, CS, SCLK, and DOUT.

    Regards,
    Brian Pisani