Part Number: DAC38J84EVM
Other Parts Discussed in Thread: DAC38J84, , LMK04828
Hello everybody,
I have some questions about interfacing with the DAC38J84.I hope you can help me or give some advice.
I am trying to interface the DAC38J84EVM board and the Xilinx KC705 FPGA using the JESD204b interface. I am using the onboard LMK clock for JESD and FPGA clock generation.
The logical FPGA core is transmitting data and SYNC is asserted, after triggering SYSREF, but i always get 'FIFO read error' and 'FIFO read empty' high, even after clearing and reading them when the link is established. No data is output from any of the DACs.
I tested the DAC with the internal NCO and can confirm normal operation.
Can this be a problem with the initialization sequence?
The JESD parameters are as follows:
FPGA: Xilinx K705 using Xilinx JESD204B IP core
L=4, M=4, F=2, K=10, S=1, HD=0
DAC input rate: 122.8 MSPS
interpolation: 2
FPGA ref = FPGA core clk = 245.76 MHz
Also attaching the DAC config file.
Hoping for some help
Thank you,
Ignas
LMK04828 0x00 0x00 0x02 0x00 0x100 0x18 0x101 0x55 0x103 0x01 0x104 0x20 0x105 0x00 0x106 0xF0 0x107 0x11 0x108 0x63 0x109 0x55 0x10B 0x01 0x10C 0x20 0x10D 0x00 0x10E 0xF0 0x10F 0x76 0x110 0x08 0x111 0x55 0x113 0x00 0x114 0x00 0x115 0x00 0x116 0xF9 0x117 0x00 0x118 0x18 0x119 0x55 0x11B 0x00 0x11C 0x20 0x11D 0x00 0x11E 0xF9 0x11F 0x00 0x120 0x10 0x121 0x55 0x123 0x00 0x124 0x00 0x125 0x00 0x126 0xF9 0x127 0x11 0x128 0x08 0x129 0x55 0x12B 0x00 0x12C 0x00 0x12D 0x00 0x12E 0xF9 0x12F 0x00 0x130 0x08 0x131 0x55 0x133 0x00 0x134 0x20 0x135 0x00 0x136 0xF9 0x137 0x01 0x138 0x00 0x139 0x02 0x13A 0x00 0x13B 0xA0 0x13C 0x00 0x13D 0x08 0x13E 0x03 0x13F 0x00 0x140 0x00 0x141 0x00 0x142 0x00 0x143 0x12 0x144 0xFF 0x145 0x00 0x146 0x10 0x147 0x1A 0x148 0x02 0x149 0x42 0x14A 0x02 0x14B 0x16 0x14C 0x00 0x14D 0x00 0x14E 0xC0 0x14F 0x7F 0x150 0x03 0x151 0x02 0x152 0x00 0x153 0x00 0x154 0x78 0x155 0x00 0x156 0x7D 0x157 0x00 0x158 0x96 0x159 0x06 0x15A 0x00 0x15B 0xD4 0x15C 0x20 0x15D 0x00 0x15E 0x00 0x15F 0x0B 0x160 0x00 0x161 0x01 0x162 0x44 0x163 0x00 0x164 0x00 0x165 0x08 0x166 0x00 0x167 0x00 0x168 0x08 0x169 0x59 0x16A 0x20 0x16B 0x00 0x16C 0x00 0x16D 0x00 0x16E 0x13 0x17C 0x15 0x17D 0x0F DAC_RESET 0x00 0x1 DAC3XJ8X 0x00 0x0118 0x01 0x0003 0x02 0x2002 0x03 0xA300 0x04 0xF0F0 0x05 0xFF07 0x06 0xFFFF 0x07 0x2C00 0x08 0x0000 0x09 0x0000 0x0A 0x0000 0x0B 0x0000 0x0C 0x0400 0x0D 0x0400 0x0E 0x0400 0x0F 0x0400 0x10 0x0000 0x11 0x0000 0x12 0x0000 0x13 0x0000 0x14 0x0000 0x15 0x0000 0x16 0x0000 0x17 0x0000 0x18 0x0000 0x19 0x0000 0x1A 0x0000 0x1B 0x0000 0x1E 0x9999 0x1F 0x9980 0x20 0x8008 0x22 0x1B1B 0x23 0x01FF 0x24 0x0020 0x25 0x2000 0x26 0x0000 0x2D 0x0001 0x2E 0xFFFF 0x2F 0x0004 0x30 0x0000 0x31 0x0400 0x32 0x0000 0x33 0x0000 0x34 0x0000 0x3B 0x0000 0x3C 0x0028 0x3D 0x0088 0x3E 0x0128 0x3F 0x0000 0x46 0x1882 0x47 0x01C8 0x48 0x3143 0x49 0x0000 0x4A 0x0F01 0x4B 0x0801 0x4C 0x0903 0x4D 0x0300 0x4E 0x0F0F 0x4F 0x1C61 0x50 0x0000 0x51 0x00DC 0x52 0x00FF 0x53 0x0000 0x54 0x00FC 0x55 0x00FF 0x56 0x0000 0x57 0x00FF 0x58 0x00FF 0x59 0x0000 0x5A 0x00FF 0x5B 0x00FF 0x5C 0x1133 0x5E 0x0000 0x5F 0x3210 0x60 0x5764 0x61 0x0211 0x64 0x0003 0x65 0x0003 0x66 0x0003 0x67 0x0003 0x68 0x3D0F 0x69 0xFF0E 0x6A 0xD50B 0x6B 0x190E 0x6C 0xF007 0x6D 0x0060 0x6E 0x0000 0x6F 0x0000 0x70 0x0000 0x71 0x0000 0x72 0x0000 0x73 0x0000 0x74 0x0000 0x75 0x0000 0x76 0x0000 0x77 0x0000 0x78 0x0000 0x79 0x0000 0x7A 0x0000 0x7B 0x0000 0x7C 0x0000 0x7D 0x0000