Part Number: DAC39J84
Other Parts Discussed in Thread: LMK04828,
Hi deer TI
I use LMK04828 to supply device clock and SYSREF to DAC39J84 on my own board. There are some questions about the setup time between device clock and SYSREF.
1.My JESD204B configuration is LMF = 841 HD =1 k =32. My device clock = 600MHz, SYSREF = 9.375MHz. The frequency of device clock is much higher than SYSREF. There is no doubt that SYSREF will be sampled by device clock. In other words even though the first rise edge of device clock doesn't sample the SYSREF ' high level. There must be a rise edge of device clock can sample the SYSREF ' high level after the first one. Is it necessary to set the setup time between Device clock and SYSREF.(As the data sheet of DAC39J84 setup time =50ps)
2.Whether DAC39J84 just only recognize the first rise edge of device clock to sample the SYSREF? If the first rise edge of device clock doesn't meet the setup time requirement whether the next rise edge that can sample the sysref also can not be recognized by DAC39J84.
Regards
Zhipeng