Part Number: TSW14J50EVM
Other Parts Discussed in Thread: ADC12J4000
Hello,
is the complete source code for the Firmware (bitstream and C-code) available to customers?
I want to read out an ADC12J4000 at full speed (preferably) and was looking at TSW14J50 or TSW14J56. However I am a bit concerned if this hardware would be easy to manipulate for further applications or if it is basically limited to the capture function due to the low-end FPGAs on the boards? I basically want to do some data processing with the 4GSPS data stream, send out data via SPI. I and am looking for an affordable solution to achieve that.
Regards, Rolf