Part Number: ADS1198
Other Parts Discussed in Thread: ADS1194,
We have started using ADS1194 with 3.3v DVDD and internal 2.048 MHz clock.
In all my questions I am referring to ADS1198 datasheet with headline, page/figure numbers.
Q1-P.27 fig.28
"In read data continuous mode , the DOUT output line also indicates when new data are available. This feature can be used to minimize the number of connections between the device and the system controller."
Does this mean we don't need to monitor DRDY? Please explain the behavior of DOUT.
Q2- P.36 RDATAC
In Figure 38,
CS is not de-activated after the frist data is sent, should we keep CS active all the itme or only when we have a SPI transaction??
Why DOUT goes high for tUPDATE after frist data is sent? What is that glitch?
Q3- P.30 Fig.33
Please explain figure 33,

Why when Start pin goes low, DRDY is activated after tSDSU??? Shouldn't de-activate because conversion is stopped?
Why when START deactivates, DRDY is still active??