Part Number: ADS1198
Q1-Is settling time required "only once" at the beginning when START is activated? Is tSETTLE=3xtDR or it's from Table 7? These 2 don't match.
Q2-In ADS1198 datasheet P.29 under Settling Time it says:
"Note that when START is held high and there is a step change in the input signal, it takes 3 × tDR for the filter to settle to the new value. Settled data are available on the fourth DRDY pulse."
What does it mean by fourth DRDY pulse?? Please explain.
Q3-Is the timing on Figure 31. correct?
Data is ready every tSettlingTime=3xtDR, so DRDY should go low every tSettlingTime=3xtDR because it takes tSETTLE for any conversion to settle?