This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1198: Data format and range

Part Number: ADS1198
Other Parts Discussed in Thread: ADS1194,

Q1- In ADS1198 datasheet page 27 under Data retrieval It says output data is 24+#ch*16 bits, so for 1194 should be 24+4*16=88 bits. Should I read 88bit frames for ADS1194, or read 152bits frame but just ignore last 4 channels?

Q2- If gain is not 1, LSB weight is Vref/Gain.(2^15-1)?

Q3- In page 21 under Input Diff. Dynamic Range, it says input range is Vref/Gain, so with Vref=2.4V and Gain=6, input range is 2.4/6=400mV, but datasheet says input range is 300mV for this values. Why is that?