Part Number: ADS1248
Hi,
I'm using the ADS1248 to measure thermocouples and have some questions about the Self and System calibration modes:
I currently have the following:
AVDD = 5V
AVSS = 0V
REFP0 = 2.5V
REFN0 = 0V
1. During SELFOCAL do I need to set the MUXCAL register to 001 (Offset Calibration) or does the SELFOCAL do this automatically?
2. SYSOCAL requires the inputs to be externally shorted to a voltage near the mid-supply. As we cannot do this with any of our inputs, could we use one of the System Monitors?
3. SYSGCAL requires the inputs to be set to Full Scale. Again, we cannot do this using AIN0-7, are there any options to do this with a System Monitor?
4. If we can only do System Calibration using the System Monitors, is there any point? If the values are factory trimmed, will I actually gain any accuracy by doing a System Calibration with Systems Monitors?