Other Parts Discussed in Thread: ADS1298ECGFE-PDK
Dear all,
I am trying to use ADS1299 to acquire ECG.
I have already acquired EEG with my own demo board. I also want to acquire ECG data.I use Biasout as Right Leg Drive and set the inputs refer to the datasheet of ADS1298ECGFE-PDK as shown:
I get WCT from the average value of RA,LA,LL by a opamp adder. And I assign the WCT to BIAS_IN pin as negative input by setting CHxSET = 0x67.V1-V6 is connected to positive input.
But the channel is saturated, the data is 0x7FFFFFF or 0x800000 for V1-V6 while the LEAD I and LEAD II is good.I try to use SRB2 as input for WCT(change V1-V6 to negative input), the result is same.I can not use SRB1 as negative input because SRB1 is connected to every channel when it is set in MISC2. But the LEAD I and LEAD II need RA act as negative input.
When I connect WCT directly to negative input of the channels, I can get the V1-V6 data.Is there any problem with my settings?
Thanks.