Other Parts Discussed in Thread: TVP5146M2
I have a project that uses the TVP5146M2 Decoder and I am having an issue or I don't seem to not fully understand why I am seeing what I am seeing.
My initialization sequence after power up:
write 00 to register 02 (set video standard = auto)
write 00 to register 08 (luminance processing, trap filter)
write 04 to register 0E (chrominance filter)
write 43 to register 33 (10 bit 4:2:2 output format)
write 11 to register 34 (enable YCbCr output and clock output)
write AF to register 36 (enable HS and VS output)
After that I can receive image data at 60 frames /sec. The image data is very noisy (see picture), but it has some correlation with the real screen content.
The content of Status 1 Register (3A) is constantly changing, typical values = 13, 1B, 11, 71.
It means we have Horizontal sync sometimes, but we never have Vertical sync I believe.
The input video is NTSC, horizontal scan frequency of 15.700 kHz, 280x192 resolution. I can't foresee any issues with this except the image may be skewed off-center.
The content of Status 2 register (3B) is always 20 = signal is not weak, no color killer, no macrovision.
The content of Video Standard Status Register (3F) is 81 = the autodetected mode is (M, J) NTSC.
Register content from 00 to DF:
00 0F 00 00 23 10 00 00 00 80 80 80 00 00 04 00
80 80 80 80 80 80 55 00 25 03 00 00 40 00 04 00
07 00 01 00 15 00 00 00 CC 00 00 00 00 00 00 00
00 05 00 43 11 FF AF FF FF 00 13 20 55 06 0A 81
00 18 0D 02 00 00 20 20 20 20 00 09 00 09 00 09
00 09 00 00 1F 1F 64 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
03 00 00 19 00 12 8A 64 06 1E 40 00 00 00 00 00
51 46 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00
00 00 1E 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 06 1B FF 00 FF 00 00 00 00 00
Can someone please comment on anything I should check, other registers I need to deal with, or what my issue could be? Thanks in advance for your assistance.
Henry