This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/ADS1293EVM: ads1293evm is used to interfacing the aurdino mega 2560 is possible or not

Part Number: ADS1293EVM
Other Parts Discussed in Thread: ADS1293

Tool/software: WEBENCH® Design Tools

ads1293evm is compatible with aurdino are not , if it compatible its connecting to arduino mega to PIN SDO is possible ,sir please suggest me sir the correct method to interfacing the aurdino mega 2560 t0 ads1293evm

  • Hey rakesha,

    The ADS1293EVM is to be used for evaluation purposes only i.e. to evaluate the features and performance of the ADS1293 - the IC on the EVM. We do not support re-purposing the EVM for any other use. However, the ADS1293 communicates via SPI. It may be possible to wire the SPI port of another processor to the SPI pins on the ADS1293 to communicate with it. The details of the SPI interface of the ADS1293 can be found in the ADS1293 datasheet.

    Regards,

    Brian Pisani