Part Number: ADS1232
Dear Sir,
I am using ADC ADS1232 in my hardware for reading the load cell value in my program. I am taking 21 bits of ADC data and doing average of 16 values of these data. Then use these values for further calculation. My problem is that when I apply power supply my circuit board, I got some counts like 77563 approx in starting. But these counts will decrease automatically in some time intervals, like: 77560, 77558, 77555, 77551 etc. while there is no load apply on the load cell. Also in some times same functioning performed in increase manner like: 77565, 77568, 77569, 77571.......... and so on. The time interval in these readings is approx 20-30 seconds and also in minutes some cases.
ADC configuration I am using is as below:
Gain: 128 (Gain0 -> 5V, Gain1 -> 5V)
Speed: 10 SPS (SPEED Pin -> Ground)
Temp: Low Signal to Temp Pin
External Crystal (4Mhz) Attached on pin 3 and 4 .
So please suggest me why this behavior is occurred. Is there anything missing in my circuit?
Thanks in advance for your valuable suggestions.....
With Regards..
Anuj Jain