Part Number: ADS5409
IN datasheet of ADS5409 on page 36 is description of 3A register.
We see that in D12-D11 default is 01 (LVDS SW - 2 mA to 2.75 mA). And in D15-D13 default is 110 (LVDS output current strength - 3.5 mA).
But we see note - in D12-D11 LVDS driver internal switch setting – correct range must be set for setting in D15-D13. As we can see LVDS output current strength is set 3.5 mA, but according to bit D12-D11 it must be set 2 mA to 2.75 mA, not to 3.5 mA.
Is an error in the document for this register description?