Part Number: ADC12D1800
Does this ADC perform acceptably when sampling a non RF waveform (so not a sine wave). I want to sample a signal composed of random high speed "pules".
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC12D1800
Does this ADC perform acceptably when sampling a non RF waveform (so not a sine wave). I want to sample a signal composed of random high speed "pules".
Hi Dan
Yes. The ADC12D1800 family devices work well with non-sinusoidal signals. The key is to maintain the input common mode voltage within the specified range.
If the pulses are asymmetrical or not 50% duty cycle then you will probably need to use a DC-coupled differential amplifier as the driver. The amplifier output stage will need to be biased at the proper common mode voltage using the ADC Vcmo pin. Table 6-6 in the ADC12D1800 datasheet has a few example differential amplifier choices to fit different needs.
Best regards,
Jim B