Other Parts Discussed in Thread: ADS5463, ADS5463EVM, ADS54RF63EVM, ADS54RF63
Hello,
I am running into a nasty glitching problem with ADS5463. After spending quite a bit of time looking for some problem in my hardware or logic I am convinced the issue is in the converter itself.
Here is what I am doing. I apply 500 MHz clock and 6.25 MHz (500/80) sinewave signal to the ADC. The two signals come from HP8664A and HP8662A respectively (synthesizers are locked at 10 MHz). When I acquire a snapshot of the ADC data, signal repeats every 80 samples. My analysis looks for jumps over some threshold in each of the 80 channels. I first saw the problem on my custom processing unit. Since then I have replicated the effect using ADS5464EVM (connected to Xilinx Spartan 3A Starter Kit using a custom module). The EVM is driven by 7.5 dBm clock (1.5 Vpp) and 7.2 dBm input signal. FPGA data sampling window is optimized by phase-shifting DCM clock. At +590 ps from nominal phase bit 10 produces frequent errors, and at -530 ps - bit 8.
At 500 MHz with threshold set to 15 counts, I see glitch amplitudes ranging from 18 to 80 counts. All glitches are single-point events, that is the acquired data deviates from a sinewave for only one sample. Looking at the glitch bit patterns, most involve bits 5, 6, 7, and 8 (typically multi-bit errors).
In the datasheet I see no mention of output error rates, etc. Has this been characterized? Have other people seen this? Is there something I am doing wrong? Is it likely that AD54RF63 would do better at 500 MHz?