This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VSP5611: VSP5611 analog input range

Part Number: VSP5611


Hi,

We're trying to build a camera using a CCD sensor with an output analog voltage in the range 0.5V-2.9V. I'm thinking of using VSP5611 as the AFE. But I'm confused about it's analog input range. The first page of the datasheet mentions that the input signal range is 2V. But on page 3, it is mentioned as per the image below:

The full scale range is mentioned as 1Vpp. In that case how does it support an input signal of 2V?