Other Parts Discussed in Thread: DAC8811, REF102
Hi TI Staff
Sorry to bother you.
For my project, I want to use DAC8811 EVM connected with Arduino
I have three questions for DAC8811 EVM.
First
The questions about SPI connection.
From the schematics of datasheet Page 19, the SDI, CLK is not connected with J2. They are connected or not?
Second
The question about Power Supply.
1) If I used Vcc and Vss to +(-)5V not standard 15V, the output of voltage of reference will be changed from 10V to ?V?
2)I confused about 5VA. does this mean 5V with 1A?
3) Could I use 5VA to VCC?
4) When I received the board, two grounds were connected (General and Analog Ground), Are they connected together? Or they should be connected to different GND.
Third
There is equation (2) in datasheet about calculation output voltage of bipolar.
The issue is if I input the code of FFFF, 65535 divided by 32768 and minus one is close to one not the exact one. So how can I get the accurate Apex.
Furthermore, I already built the sinwave syntax like :
unsigned int Sin_tab[256] = { 32768, 33572, 34376, 35178, ...........}
how should I efficiently change the frequency of this waveform in coding for Arduino.
How should I code in the LOOP? SPI.Transfer(Sin_tab)?
Thanks very much