Part Number: ADS131E08
Hi,
I have a problem about SPI interface, spesifically DOUT line. I was able to read and write registers of ADS131e08 but when i put the device into continious read mode i can't get the data at DOUT line into my MCU through MISO line. As you can see in Figure-2, when i don't connect DOUT to MISO and observe the DOUT line , it seems DOUT transmits data. When i connect DOUT and MISO ADS131e08 stops. After connection i send a reset and put device into continious read mode and observe Figure-3. DRDY works but there is no data on DOUT line.
I applied power-up sequence in datasheet Figure:53.
Analog Supply:5V Digital Supply:3V (Unipolar Supply)
CS is tied low after reset pulse. (I didn't selectively Pulled Low Before sending commands or reading data)
SPI Baud Rate : 1.5 MHz
MCU SPI mode is Full-fuplex master. (cpol=0, cpha=1)
MCU MISO pin is "alternate function push pull mode".
MCU GND is connected DGND.
You can see schematic in Figure-1 (Designed according to ADS131e08 user guide)
Any help or offer or information about DOUT line will be appreciated.
Thank you.
Figure-1 : Schematic of ADS131E08
Figure-2 : BEFORE (ADS131E08) DOUT--------> (MCU) MISO connection
BUS (Green) : DOUT
Digital 0 (white) : DRDY
Digital 1 (orange) : SCLK
Figure-3 : AFTER (ADS131E08) DOUT--------> (MCU) MISO connection
BUS (Green) : DOUT
Digital 0 (white) : DRDY
Digital 1 (orange) : SCLK