Part Number: DAC3171
How should the "tempdata" field of SPI Register config6, bits 15:8 be interpreted?
Is this degrees celsius? whole or fractional degrees? Signed or unsigned?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC3171
How should the "tempdata" field of SPI Register config6, bits 15:8 be interpreted?
Is this degrees celsius? whole or fractional degrees? Signed or unsigned?
Hi,
I checked with the design documentation and it says the field is an 8-bit two's-complement number that reads out the die temperature in degrees C.
Regards,
Richard P.