Part Number: TSC2003
Hello,
I am trying figure out how to read temperature using this chip. It looks like I implemented my I2C drivers correctly because I am able to measure X and Y okay and I am able to implement touch screen feature. But I could not get the right temperature readings. Any suggestions on what I am doing wrong? I am using the TM4C1294NCPDTI
void InitializeTouch(void)
{
//PENIRQ pin
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOC))
{
}//end while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOC))
GPIOPinTypeGPIOInput(GPIO_PORTC_BASE, GPIO_PIN_4);
GPIOIntTypeSet(GPIO_PORTC_BASE, GPIO_PIN_4, GPIO_FALLING_EDGE);
// GPIOPadConfigSet(GPIO_PORTC_BASE, GPIO_PIN_4, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
GPIOIntRegister(GPIO_PORTC_BASE, PortCIntHandler);
GPIOIntEnable(GPIO_PORTC_BASE, GPIO_PIN_4);
//Touch I2C pins
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C6);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_I2C6))
{
}//end while(!SysCtlPeripheralReady(SYSCTL_PERIPH_I2C6))
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOA))
{
}//end while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOA))
GPIOPinConfigure(GPIO_PA6_I2C6SCL);
GPIOPinConfigure(GPIO_PA7_I2C6SDA);
GPIOPinTypeI2CSCL(GPIO_PORTA_BASE, GPIO_PIN_6);
GPIOPinTypeI2C(GPIO_PORTA_BASE, GPIO_PIN_7);
//I2C1
I2CMasterInitExpClk(I2C6_BASE, FOSC_HZ, false);
//chip initialize
WriteTouchByte(0x90, 0x02);
PollTimer0Delay(20, 1000);
ReadTouchByte(0x90);
}//end void InitializeTouch(void)
/***********************************************/
void WriteTouchByte(uint8_t i2cAdd, uint8_t commandByte)
{
i2cAdd = i2cAdd >> 1;
I2CMasterSlaveAddrSet(I2C6_BASE, i2cAdd, false);
I2CMasterDataPut(I2C6_BASE, commandByte);
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_SINGLE_SEND);
PollTimer0Delay(50, 1000000);
while(I2CMasterBusy(I2C6_BASE))
{
}
}//end void WriteTouchByte(uint8_t i2cAdd, uint8_t commandByte)
/***********************************************/
uint8_t ReadTouchByte(uint8_t i2cAdd)
{
uint32_t i2cByte;
i2cAdd = i2cAdd >> 1;
I2CMasterSlaveAddrSet(I2C6_BASE, i2cAdd, true);
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
PollTimer0Delay(50, 1000000);
while(I2CMasterBusy(I2C6_BASE));
i2cByte = I2CMasterDataGet(I2C6_BASE);
return((uint8_t)i2cByte);
}//end uint8_t ReadTouchByte(uint8_t i2cAdd)
/***********************************************/
This is the code in my main
WriteUART0("\n\rTouch Temp1 = ");
WriteTouchByte(0x90, 0x0E);
PollTimer0Delay(20, 1000);
touchTemp1 = ReadTouchByte(0x90);
UINT32ToASCII((uint32_t)touchTemp1);
WriteUART0(decimal_string);
WriteTouchByte(0x90, 0x02);
PollTimer0Delay(20, 1000);
ReadTouchByte(0x90);
PollTimer0Delay(5, 1);
WriteUART0("\n\rTouch Temp2 = ");
WriteTouchByte(0x90, 0x4E);
PollTimer0Delay(20, 1000);
touchTemp2 = ReadTouchByte(0x90);
UINT32ToASCII((uint32_t)touchTemp2);
WriteUART0(decimal_string);
WriteTouchByte(0x90, 0x02);
PollTimer0Delay(20, 1000);
ReadTouchByte(0x90);
Temperature = touchTemp1 * 2.5 / 255 * 1000.0 * 25.0 / 600;
WriteUART0("\n\rTemp0(C) = ");
DoubleToASCII(Temperature);
WriteUART0(decimal_string);
Temperature = (2.573 * (touchTemp2 - touchTemp1) * 2.5 / 255 * 1000) - 273;
WriteUART0("\n\rTemp1(C) = ");
DoubleToASCII(Temperature);
WriteUART0(decimal_string);
This is what I see on hyperterminal. And no matter what the temperature around is, it's always like this.
Touch Temp1 = 76
Touch Temp2 = 92
Temp0(C) = 31.04
Temp1(C) = 130.60
Thanks.
AJ