Other Parts Discussed in Thread: AFE5805
Hello,
Im currently working with a TSW1400 EVM along with the AFE5805 EVM to capture ultrasound
signals. So far I am only using 1 channel and 4096 samples, which is sufficient for my project.
Ill first explain how I want the system to work. Since the purpose of this work is for an
automated signal capturing system we want it to work with fewer human interaction as possible,
so much of the information displayed on the HSDCPro software is not needed. I want to capture
data with an external trigger signal at around 1-5kHz. As mentioned before I have no interest on
the FFT, just the raw ADC data. A large amount of data from various acquisitions should be
either stored on memory (1GB DDR2) for later retrieval or the data should be constantly
transferred as it is captured to the PC and stored on a HD (without displaying the time domain
and FFT graphs on the HSDCPro software).
The problem Im facing is the time it takes to capture a single data, as it should send the
capture command, retrieve data from memory, send it back to the PC via USB, calculate the FFT
and plot both time domain and FFT graphs on the HSDCPro software.
I also explored the "HSDCPro Automation DLL" fodler which contains the .dll for MATLAB, C or
LabVIEW code customization, but when using the "Read_DDR_memory" fuction with the external
trigger option from the DLL (or the normal capture mode without trigger) the HSDCPro graphs are
always updated to the last capture. This way Im unable to capture data at a 1-5kHz rate as I
require it.
As mentioned in
e2e.ti.com/.../1022451
the TSW1400 was made to run along a computer and the HSDCPro software. So the HSDCPro is
indispensable to work with the TSW1400? My colleague emailed a TI engineer a few weeks ago
asking for the HSDCPro LabVIEW source code but was denied it.
I was wondering if the solution to my problem lies in the .rbf firmware file loaded into the
FPGA or is it in modifying the .dll (if it is possible) file.
I hope I was clear on my explanation and would appreciate any enlightenment. Thanks for spending
your time reading this.
Regards,
Guilherme O.