Part Number: ADS1118
Hello,
Regarding to configuration register(datasheet page25) on ADS1118, my customer is asking a question.
(Question)
If bit0(reserved) is set as “1” or “0”, is there any impact in device?
I think that generally, even though the read only bit is written to 0 or 1, the device won’t be the influence.
But I know that the read only bit prohibits from writing depending on device.
So I am asking that ,just in case.
Regards,
Tao2199