This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS42B49EVM: Sampling and data processing FFT question

Part Number: ADS42B49EVM

Heys everyone,

I'm waiting for my ADS42B49EVM to arrive, so I've started researching (codewise) about how to implement the processing of the data adquisition of a certain signal. The thing is that I've been checking the CMSIS DSP library to use with, however, I'm having some difficulty understanding how this algorithm can actually be used to process all the data I'll acquire. 

The signal being processed is a 10MHz signal, therefore I'm going to sample at a frequency of 50MHz (50MSPS) to have a nice signal precision and resolution. 

My question rises after thinking about this: If I have 50MSPS (let's say my signal needs to be processed every 5ms):

5ms/1000ms = 0.005.

50 000 000 * 0.005 = 250 000 samples exist in those 5ms.

If I want to do a spectral analysis, and process every 5ms those 250 000 samples using an FFT; how can I use the CMSIS DSP library's FFT function?

I ask this since the limit for the function is 4096, and documentation says that the output gives the DC component, fundamental frequency, first harmonic, etc. but if I get 4096 values from the ADC (ADS42B49EVM), then process them by doing an FFT, I wouldn't have enough data to check if the frequency changed in that time lapse wouldn't I (because there would only be the first 4096 samples considered, and what about the other 245 904 samples?)

Any advice or suggestion to guide me on this?

I'm pretty confused  on how to implement this, and questions just keep rising.

Thank you, Alan.