Part Number: ADS8528
I would like to use multiple devices in parallel mode sharing a bus, simultaneous capture on all. Are the digital data/other lines high impedance when CS is high for each device, such that CS can be used to select which device to read data from? And when CS is high for programming the registers, if all devices share the same HW/SW and RD/WR and data lines will they all be programmed at the same time for the same mode? Or is a tri-state buffer required for this approach.