Other Parts Discussed in Thread: ADS1298
I have used two seperate ADS 1298 chips and both of them lasted for little over a week. The moment I try to connect the reset pin I get a short circuit with 93 mA current on my power supply. I am not sure if there is a problem with the ADS 1298 chips or something I am doing wrong. It could be the ESD problem but I am worried since both of them just lasted for 1 week.
Also when they were working fine when I had programmed the first 14 registers
| 1 | Config 1 | 38d | ||
| 2 | Config 2 | 32d | ||
| 3 | Config 3 | 201d | ||
| 4 | Lead-off | 0 | ||
| 5 | CH1SET | 1 | ||
| 6 | CH2SET | 1 | ||
| 7 | CH3SET | 1 | ||
| 8 | CH4SET | 1 | ||
| 9 | CH5SET | 1 | ||
| 10 | CH6SET | 1 | ||
| 11 | CH7SET | 1 | ||
| 12 | CH8SET | 1 |
When I read all registers I got the 201 as 200. I also read all other register values which should give me default values but the RESP and WCT2 I get as zero which are not by deault zero.