Hi,
Our design involves two main boards; a 'core' module which contains the DM365, SDRAM, NAND and supply circuitry and a 'gateway' module onto which the 'core' module plugs via dual row 1.27mm pitch header pins and contains the TVP5146 Video Decoder, Micrel Ethernet Phy, battery backup etc. The goal with this was to confine the high speed routing and minimize the size (/expense) of a highly multilayer board of & reusable & modular 'core' module.
My question revolves around an uneasiness I have regarding taking the TVP5146 off the 'core' module and onto the lower 'gateway' module. This requires the tracks (YIN7 through YIN0, CIN7 through CIN0, and HD, VD, C_WE_FIELD & PCLK) being fed down through the 1.27mm pitch double header connector down to the gateway board before it is routed to the TVP5146 & the RCA connectors. Ie the tracks from the DM365 to the TVP5146 are longer than the tracks from the RCA connector to the TVP5146.
I have two options: TVP5146 close to the DM365 or TVP5146 close to the RCA connector. Logically, the highest frequency the raw analog video lines will carry for PAL, SECAM or NTSC will be around the 7MHz mark (correct?) whilst the BT.656 lines will be around the order of 13.5Mhz (Page 17 of SLES141D for the TVP5146) (correct?). I would prefer to keep the TVP5146 on the lower 'gateway' module. Would anyone care to entertain my concern and provide some input re the dangers of extending either the digitized or the raw analog lines or whether I should be concerned at all?
Many thanks,
NickA