Part Number: ADS1298
Other Parts Discussed in Thread: ADS1294
Hi,
I am going through the data sheet of ADS1298. I have the following queries:
1. What are the basic difference between the different members of the ADS129x series?
2. The input referred noise is 4 μVPP (150 Hz BW, G = 6).
i) What does G stand for?
ii) Considering the max voltage =5.25V. A 24 bit ADC would require an noise which is less than 5.25/(2^24) V , which is equal to 0.3μ. Please explain with the calculations involved??
iii) What is the reference volatge for the sigma delta modulator ??