This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/ADS1292R: Modded behringer x32 with external preamps

Part Number: ADS1292R

Tool/software: Code Composer Studio

hi guys!
after touring for about 3 years with a stock x32, I felt that I can improve the sound so I decided to mod it. now it has the preamps completly removed from the signal chain and the conveters upgraded (better capacitors, different opamps). http://amthanhthudo.com/loa-line-array
now I m using it with an api 3124 and 8 ch of api clones (they re not 100% clones since they have different trafos, haufe and neumann).
when using this setup I found myself using a lot less eq, everything was sitting better in the mix. also I felt that the transients were much faster.
here are some drums tracked with it. beta 91 on bd, i7 snare, 57 on tom, 421 on ft, 414 oh.
no eq used, only a hpf for oh (I think at about 100, there was a lot a bass on stage from the pa)