Other Parts Discussed in Thread: ADCPRO, ADS124S08EVM
The device does not enter the "sleep" low power state when the conversion completes. I see Idd = 174uA with START pin low. Vrefout is disabled after the conversion completes. The A/D is sampled every 8 seconds (first column below). MOSI, MISO are the last two columns below
8.270505600000000,3,0x40,0x00
8.270511360000000,3,0x06,0x00
8.270517280000000,3,0x13,0x00
8.270523040000000,3,0x00,0x00
8.270528799999999,3,0x60,0x00
8.270534560000000,3,0x02,0x00
8.270540320000000,3,0xDD,0x00
8.270546080000001,3,0xFF,0x00
8.270551840000000,3,0xFF,0x00
8.270557600000000,3,0x4A,0x00
8.270563520000000,3,0x01,0x00
8.270569280000000,3,0x07,0x00
8.270575040000001,3,0x8C,0x00
8.271660960000000,4,0x04,0x00
8.271666720000001,4,0x04,0x00
8.322542720000000,5,0xFF,0x1C
8.322548480000000,5,0xFF,0x49
8.322554240000001,5,0xFF,0x12
16.270427680000001,6,0x40,0x00
16.270433440000001,6,0x06,0x00
16.270439199999998,6,0x13,0x00
16.270444959999999,6,0x00,0x00
16.270450719999999,6,0x60,0x00
16.270456480000000,6,0x02,0x00
16.270462240000001,6,0xDD,0x00
16.270468000000001,6,0xFF,0x00
16.270473920000001,6,0xFF,0x00
16.270479680000001,6,0x4A,0x00
16.270485440000002,6,0x01,0x00
16.270491199999999,6,0x07,0x00
16.270496959999999,6,0x8C,0x00
16.271582720000001,7,0x04,0x00
16.271588640000001,7,0x04,0x00
16.322463519999999,,0xFF,0x1C
16.322469280000000,,0xFF,0x49
16.322475040000000,,0xFF,0x2E