Other Parts Discussed in Thread: ADS52J90EVM, ADS52J90, AFE58JD18, AFE5818, LMK04806
Hello all,
I would like to create a 16 channel DAQ (12 bit or 10 bit are both fine) with a high sampling frequency. I learned that if I use TSW14J56EVM in conjunction with ADS52J90EVM, that will do the job (in fact I learned that I should use FMC boards). Actually, I may want a 32 channel DAQ in the future and I thought this combination will do that for me.
Here are my questions:
1. Will this combination be able to acquire 10 MHZ signal for the duration of 100 us every 10 ms (I have a trigger)? This event will continue for about 3 minutes.
2. Will I have to store the whole data on the internal memory of the card and once my acquisition finished, I can transfer it to a computer?
3. What other devices do I need to buy so I could make my DAQ (power supply, signal generator, etc)?
4. Is there any better pair that you could recommend?
Thank you very much