Part Number: DAC3484EVM
Hello All,
I am designing a custom board based on high speed DAC DAC3484 , using DAC348XEVM-SCH_H Schematics as a reference.
Referring the schematics , Part U2 - CDCE62005 - pin 16(U2P) : DACCLKC is connected to U1-DAC3484- pin B3 (DACCLKN)
& Similarly Part U2 - CDCE62005 - pin 17(U2N) : DACCLK, is connected to U1-DAC3484- pin A3 (DACCLKP)
This looks like P&N of the CDCE62005 is connected to N&P of DAC3484, is this right way? (Because other P&N signals coming out of DAC3484 or CDCE62005 are connected in a matched way ). Datasheet of CDCE62005 says its outputs are user definable
Please suggest at the earliest.
Thanks&Regards,
Shyamsundar