Part Number: ADS7924
Other Parts Discussed in Thread: TPS24751
Hello,
I have a couple of questions on the ADS7924
- can I combine AGND/DGND or do I need to keep them separate? if separate, they will be tied together locally with a 0-ohm
- looks like AVDD needs to be greater than or equal to DVDD – could I just use the same voltage for both(2.5V, 3.3V or 5V all meet both requirements)? or is there a benefit for separate? is it best to keep the AVDD closer to the Analog input voltage to get more resolution?
- I only plan to use 3 channels, can I leave unused floating?
- ABS max on the analog input voltage shows a max of 0.3V… is this correct, or should it be in relation to AVDD?? hopefully, since my input is from the TPS24751 it will be a full scale voltage of 675mV
Thanks!