This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8728: The current specs for REF_A and REF_B on DAC8728

Part Number: DAC8728

Hi Team,

Do you have the test data of  current specs for REF_A and REF_B on DAC8728? I can't find it from datasheet. Please share them to me if you have it in hand. Thanks. 

BR,

Eric Jin

  • Hi Eric,

    The reference input current can be calculated from the reference voltage divided by the input impedance. As the input impedance is 10 M Ohm (page 5 in datasheet), the current will be sub-nano amperes.

    Hope I have answered your question.

    Regards,
    Uttam Sahu
    Applications Engineer, Precision DACs