Part Number: AMC1306E25
Hi, I don't understand about the density of ones in the output bit stream.
If there are ten 1s in 100 bits, so the density is 1/10. It's also possible that we can see two 1s in 10 bits, so the density changes to 2/10. What's the period when we consider the density?
This part is compatible with the SDFM function block in C2000 MCU, right? But the clock pin in this part and C2000 MCU are all input, so we need an external clock to drive the clock pin, right? Why we do not design a clock inside and make the clock pin an output?
Thanks.