This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298ECGFE-PDK: Testing Arbitrary Signal on ADS1298ECG-FE board with C5515 EVM

Part Number: ADS1298ECGFE-PDK
Other Parts Discussed in Thread: ADS1298

Hello Ti Community,

I have C5515 EVM and ADS1298ECG-FE. I have gone through the PDF containing ECG implementation on ADS1298 using C5515 DSP.

I actually want to test the working of the code i got from the link in the pdf document. Now I as i dont have an ECG simulator or J15 cord for 12 lead ECG input configuration of that kind, I am planning to test the working of the code using a sine wave of say 100 Hz. I am generating the sine wave from an Arduino UNO. Can you show me the the hardware configuration for where i should connect the signal.

I've tried removing 16jumpers from J27 to J33 on ADS1298ECG-FE board and i shorted all the positive and negative terminals and connected it to input signal of 100 Hz sine wave. The problem I faced in this configuration is that while i run the code in CCS, the compiler goes to the isr of INT1 (in  InterruptHandlers.c), but I am unable to get the data from FE to C5515 EVM.

So please help me, whether I got the hardware configuration wrong. Or is there any other way to test a single sine wave using ADS1298 FE and C5515 EVM.

Ketan Shirokha

Electrical Engineering, IIT Bombay