This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150AM1: How to setup 7.5IRE ?

Part Number: TVP5150AM1


Dears,

We use the AM5150AM1 as the Video Decoder.

We want to set 7.5IRE for NTSC-M and 0 IRE for PAL/NTSC-J.

We try to use the register 07h[6]: "Pedestal not present" to set the IRE selection, but we find it is useless!

It seems always in 0 IRE whatever we set 07H[6] = 1'b0 or 1'b1.

Does any other register need to be enabled to apply the 07H?

Could you give us some suggections to how to setup 7.5IRE ?

Thanks you.

Best regards,

Maxli

  • Just curious... are you trying to decode a non-standard video signal?

    The TVP will usually detect the correct video format and automatically adjust the digital output range to correspond to the source analog video format.

    Usually the only time you need to force the pedestal setting is if you have a non-standard signal.

    How are you determining that the pedestal setting is having no effect?

    BR,

    Steve

  • Hi Steve,

    We use the pattern generator ASTRO-VG872C and the SMPTE color bar as test pattern to check the black level. The three dark bar should be superdark(0 IRE), dark(7.5IRE) and gray.

    So, if we use NTSC-M and set pedestal(7.5IRE), we should only see two dark bar at lower right.

    We always see the three bar whatever the register 07h[6] is one or zero, so it seems the registers is useless.

    Could you give us some suggestions? or how to debug the issue?

    Thank you,
    BR,
    Maxli
  • Do the digital video data values change when you toggle the pedestal register?

    BR,
    Steve
  • Hi Steve,

    We use the NTSC-M and full black screen to read the digital data values of YUV422.
    They are alwyas the "19 80 20 80" when we toggle the pedestal register! (0x60 switch to 0x40 and switch to 0x60)
    We also write the pedestal register then read back to check the value.

    We dump all the TVP reigsters for you.
    "r" means the reserved and skip to read it.
    =======================================================================
    - : 0 1 2 3 4 5 6 7 8 9 a b c d e f
    0 : 0 15 0 6d 0 0 10 40 0 80 80 0 80 47 0 a
    10 : 0 0 0 0 0 25 5f 80 0 0 c 14 0 0 0 r
    20 : r r r r r r r r 0 r r r 99 6d r r
    30 : 0 r r r r r r r r r r r r r r r
    40 : r r r r r r r r r r r r r r r r
    50 : r r r r r r r r r r r r r r r r
    60 : r r r r r r r r r r r r r r r r
    70 : r r r r r r r r r r r r r r r r
    80 : 51 50 4 0 2 d df 0 e 28 18 2 81 r r r
    90 : 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    a0 : 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    b0 : 3a 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    c0 : 80 0 4 r r r r r r r r r r r r r
    d0 : r r r r r r r r r r r r r r r r
    e0 : r r r r r r r r r r r r r r r r
    f0 : r r r r r r r r r r r r r r r r
    =======================================================================

    Thank you,

    Best regards,
    Maxli
  • Hi Steve,

    The same issue is in PAL / NTSC-J.
    We also use the full black screen, the digital value is "11 80 10 80" whatever the pedestal register is 1 or 0 .
    So, it seems that TVP detect the black level automatically without reference to the pedestal reigster setting.

    Please help us to check the TVP registers in previous message.

    Thank you,

    Best regards,
    Maxli
  • Hi Steve,

    Do you have any update ?

    Best regards,
    Max
  • Sorry for the delayed response.

    I have been trying to find someone to help clarify this issue but unfortunately this device is NRND (Not Recommended for New Designs) and as such detailed expert knowledge resources are no longer available.

    BR,

    Steve

  • Dear Steve,

    Thanks for your help.

    Best regards,

    Max

  • Hi Max,

    As far as I can tell, toggling between 0x40 and 0x60 does not alter the pedestal bit, which is bit 6, but rather you are altering bit 5. In both of 0x40 and 0x60 the pedestal presence bit is set to 1. To toggle the bit off, you will have to switch between 0x60 and 0x20.

    Thanks,

    Chris
  • Hi Chris,

    Thank you!

    You are right! I made a big mistake..

    The pedestal setting is bit 6 , it should be mask 0x40, not set 0x40.

    We set register 07H is 0x20 to check the black level of the NTSC-M and it is workable.

    Best regards,

    Max

  • Good catch Chris. :-)

    Sometimes the problems are not nearly as complicated as expected and solutions simple !!!

    BR,
    Steve
  • Dear Steve & Chris,

    We sholud check the register settings again to find the obviously mistake.

    Thanks for your useful support again!

    The issue can be closed!

    Best regards,

    Max