Other Parts Discussed in Thread: CDCE72010
Hi,
With respect to the user guide slwu061a (page 13), I was wondering if this 4th option might work:
In the VCXO pad, instead of using a VCXO, I would solder on a low jitter (<0.4ps) VCO (not VCXO) clock of 200MHz with the same footprint and pin-to-pin match to the TCO-2111T. I would also cut the feedback trace from the Loop Filter to the VCXO and keeping the original factory setting of the CDCE72010 for the Output Divider (P) of 4 --> ie 200MHz in...and 50MHz out. I'm not concerned with syncing the ref clock.
Thus, I won't have to configure the EEPROM and still use a differential LVPECL clock. This would work only if the CDCE72010 passes through the clock independent of the feedback.
Will this work? Or does the CDCE72010 lock up if I don't use a reference clock and I don't use the feedback mechanism?
Thank you.