Hello all,
A student is working on the TLV5620 and he is facing the following problem,
" The part is outputting non zero voltage on entering 0 code and the output doesn't change until about value 50 when in normal mode and 25 when in double range mode. I have a 10k pulldown on the dac outputs as per the datasheet and also buffer the outputs so no excessive currents are drawn. VDD and REFs are both 5v. "
I think, according to the datasheet recommended VDD is 3.3 and VREF is VDD - 1.5. Could it be this problem or anything else.
Could anyone help me with this.
thank you in advance.