This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7040: Roadmap for small size and internal input buffer ADC

Guru 19685 points

Part Number: ADS7040

If there Roadmap or Lineup for small size and internal input buffer ADC, Please let me know.

For example, customer hope internal input buffer version of ADS7040.

But I didn't find near device.

【Request spec】

・Logic level:1.8V

・Resolution:enough to 8bit

・Sampling rate:enough to DC level

・Small size:as small as possible

Best regards,

Satoshi