This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A04EVM: State machine and error handling for the ADC ADS131A04, C-Code available?

Part Number: ADS131A04EVM
Other Parts Discussed in Thread: ADS131A04, TM4C1294NCPDT

Support Path: /Tools & software/Help me with an issue/Design Kits / Evaluation Modules / Boards/Software issue/

We bought two ADS131A04EVM Boards and at the moment we are testing the ADC131A04 with the GUI on the PC.

On the ADS131A04EVM Board the communication runs between the ADC131A04 and the microcontroller MSP430. The MSP430 is connected to the PC over the USB interface.

We want to use the ADS131A04 in a new application and we have to implement the state machine for the configuration, data processing and the error handling.

Is it possible to get the C-Code which is implemented in the MSP430?

  • Hello Michi,

    Thanks for your post!

    I think you meant to ask about the TIVA microcontroller on the ADS131A04EVM, not MSP430. The EVM uses the TM4C1294NCPDT. Unfortunately, we do not have the source code to share for this EVM.

    Best Regards,