Other Parts Discussed in Thread: ADS8684, ADS8684A
Hello,
We are working on the design of data acquisition system.
Specifications are:
1. Number of analog input channel 4 ch. (single ended 4ch., differential 2ch.)
2. Input Range -10V to +10V, 0 to +5V.
3. Limit frequency (3dB) 10kHz/Through(200kHz) selectable (if possible)
Could you suggest any ADC that supports these specifications?
Alternatively, could you provide solution to this design.
Best Regards,
Sarang Suryawanshi