Part Number: DAC8775
Other Parts Discussed in Thread: , DAC8760
I have some questions about DAC8775
1. Is is possible to control full functionality of DAC8775 with 4-wire SPI interface(SCLK, SDIN, SDO, SYNC\) ? or LDAC\, CLR, RESET\, ALARM\ signals also should be connected to controller ?
2. In DAC8775EVM schematic, IOUT_x and VOUT_x are combined and VSENSEP_x, CCOMP_x are connected to this pins. (please check the DAC8775EVM board schematic). I want to use VOUT_x and IOUT_x separately (as a separate channels). kindly let me know the connection for VSENSEP_x, CCOMP_x and protection circuit for IOUT_x AND VOUT_x.
3. In DAC8775EVM schematic Input supply voltage is converted to fixed 12V and given to DAC8775 (AVDD/PVDD) chip. Is it possible to connect directly 28V DC to DAC8775 (AVDD/PVDD) without much changes in power dissipation and performance.