This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC14X250EVM: Can I use lower frequency signal for the clock input than presented in the user's guide?

Part Number: ADC14X250EVM
Other Parts Discussed in Thread: ADC14X250

Hello, experts.

The user's guide (SLAU625–November 2015) describes that set a clock input signal generator for 250 MHz and use it as the CLK input for ADC14X250, but unfortunately only 50 MHz signal generator is available for me.

So can I use 50 MHz clock input signal for the ADC?

Thank you in advance! :)