Part Number: DAC37J82
Can it be confirmed that the DAC37J82 does work without SYSREF?
It claims to support Subclass 1 but allows disabling use of SYSREF. Has this operation been confirmed?
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC37J82
Can it be confirmed that the DAC37J82 does work without SYSREF?
It claims to support Subclass 1 but allows disabling use of SYSREF. Has this operation been confirmed?
Mike
Michael,
The digital blocks such as NCO, JESD, clock dist, all need to be reset after they have been configured. This is done by issuing SYSREF pulses. Due to the architecture of the design, the part requires at least 2 pulses of the SYSREF input. See the attached document for more information.
Regards,
Jim
2335.DAC3xJ8x Device Initialization and SYSREF Configuration.pdf
Mike,
The JESD state machine and clock divider block can only be reset by the SYSREF signal. This information will be added to the next release of the data sheet and any mentioning of being able to operate without SYSREF will be removed.
Regards,
Jim
Jim,
Can the SYSREF pulse extend across multiple DACCLK_P rising edges and still be one pulse?
That is, are the SYSREF transistions important or just SYSREFs value on rising DACCLK_Ps?
More importantly I assume we can set the "use next single SYSREF pulse" for each of the DAC subsystems and it won't care about the length of the SYSREF pulse?
Mike
Mike,
The DAC uses the rising edge of SYSREF so the pulse width will not matter as long as it is not shorter than a multi-frame period (per the standard) if you plan on turning it off. If you leave it running, it will have to be the same frequency as the multi-frame clock or an integer divide of this value.
Regards,
Jim