Part Number: DAC3164
Other Parts Discussed in Thread: DAC3161, DAC3174
.
Champs- got a customer who is bringing a board up and we have a few questions-
1. The config20 register allows setting allows the DAC output to be set to a static value. I expected that the static value would be output on both channels of the DAC. However, the behavior I am seeing is that the “sifdac” value is only output on channel A and channel B outputs 0V differential. I don’t know if this is expected or if I am misconfiguring something. Can you confirm that this is the expected behavior?
2. The config3 register allows adjustment of the LVDS clock and data delays. Based on my experimentation, it appears that the DAC3164 uses only the ‘datadlya’ and ‘clkdlyb’ fields. The ‘datadlyb’ and ‘clkdlya’ fields do not appear to have any effect. Can you confirm whether this is the case?
Thanks in advance!