Part Number: DAC37J82
Other Parts Discussed in Thread: DAC37J84
The DAC37J82 is being used with the following Serdes configuration:
LMF = 421, S=1, HD=1, interp = 1. DAC PLL is bypassed.
When following the Initialization steps in section 8.3 in the data sheet, step 12 calls for checking the SERDES PLL lock status. This check returns 0 for both rw0_pll and rw1_pll. Is this expected considering lanes 7:4 are not being used (rw1_pll)?
Are there other things that can be checked at this point to verify that things are in a good state?